Technical FAQs

Ask a Question

Do Compact INS/INV switch-disconnectors comply with the electromagnetic compatibility standards.

The Compact INS/INV switch-disconnectors comply with the following electromagneticcompatibility standards:
> IEC/EN 61000-4-2 - electrostatic immunity discharge test
> IEC/EN 61000-4-3 - electromagnetic-field immunity test
> IEC/EN 61000-4-4 - electrical fast transient/burst immunity test
> IEC/EN 61000-4-5 - surge immunity test
> IEC/EN 61000-4-6 - immunity to conducted disturbances, induced by radiofrequency fields
> CISPR 11 - radio-frequency conducted and radiated emission tests required for
CE marking:
> EN 61000-6-2 - immunity standard for industrial environments
> EN 50081-1-2 - emissions in commercial and industrial environments
Was this helpful?
What can we do to improve the information ?