Technical FAQs

Ask a Question

Does Compact INS/INV switch-disconnectors comply against electromagnetic or mechanical vibrations.

The Compact INS/INV switch-disconnectors are guaranteed against electromagnetic or mechanical vibrations.
Tests are carried out in compliance with standard IEC 68-2-6 for the levels required by merchant-marine inspection organisations (Veritas, Lloyd’s, etc.):
>  2 to 13.2 Hz: amplitude ±1 mm
> 13.2 to 100 Hz: constant acceleration 0.7 g.
Was this helpful?
What can we do to improve the information ?