Technical FAQs

Ask a Question

What is the altitude derating for Compact INS/INV switch-disconnectors.

The Compact INS/INV switch-disconnectors are designed to operate at their rated values at altitudes under 2000 metres.
Above 2000 metres, the changes in the characteristics of the ambient air (electrical resistance, cooling capacity) result in a reduction of the characteristics below.



 
Was this helpful?
What can we do to improve the information ?