Technical FAQs

Ask a Question

Is ZBY8330 marked legend for emergency stop comply ISO 13850 standard.

Emergency Stop function “logo” (triangle with exclamation point) has been added. That is why, ZBY8330 marked legend for emergency stop comply ISO 13850 standard.
See picture below:

Was this helpful?
What can we do to improve the information ?