Technical FAQs

Ask a Question

What are the MTBF values of RXG range electromechanical plug in relays.

As these plug in relay have not electronic part, MTBF data is not relevant.
We can only provide the life time of RXG which depends to the mechanical and electrical durability. For RXG relay, mechanical durability is 10000000 cycle. 
Please, refer to the catalog in attachment (see page 4, 5) there are some curves in order to determine the electrical durability of the device following the switching capacity and the use category.
"
Was this helpful?
What can we do to improve the information ?