Technical FAQs

Ask a Question

How can we put user image instead of Schneider Logo in startup of Vijeo Designer Runtime in HMI.

Setting up the Custom Startup Screen in Vijeo Designer Runtime:

1. In the Target node properties, expand the Startup Options property.
2. Check the Custom Welcome Screen check box.
3. Select the image to use for the Welcome Screen and click Open.

Please take note that Only JPEG files can be used for the Custom Welcome Screen and the JPEG image's width and height cannot be greater than your target machine's screen resolution.
Was this helpful?
What can we do to improve the information ?