Technical FAQs

Ask a Question

Do the SRC5000UXI to 10000UXI models turn ON without battery, when the input power is available?

Yes.  The SRC5000UXI to 10000UXI models will turn ON if the battery is not connected when the input power is available.
Was this helpful?
What can we do to improve the information ?