Technical FAQs

Ask a Question

What is the use of Parallel Kit for SRC5000UXI to 10000UXI models?

The Parallel Kit allows to connect the two UPS's output supply to the load through a common AC bus bar.
Both the UPS's will share the load equally when both the UPS's are working fine.
But if one UPS should fails, either through developing a fault or being taken out for maintenance, then the load will work on the other UPS.
’1+1’ parallel redundancy system is available to effectively improve the reliability of the system.
Was this helpful?
What can we do to improve the information ?