Technical FAQs

Ask a Question

How can I show values of variable tag with scaling in Vijeo Citect trend page whose range is in floating point like between 0.0001 to 1000.

To display values proper values in floating point you need to first confirm that you have configured a trend tag with storage method as "Floating Point (8 Byte Sample )".
Also you need to put the correct scaling in the variable tag configuration like Eng Zero & Full Scale as well as the format like ####.#### 
Using these values properly you can be able to read values with desired decimal points in Trends/Process Analyst page .
Kindly check the attached snapshot for configuration details.
Was this helpful?
What can we do to improve the information ?