Technical FAQs

Ask a Question

With Vijeo Citect 7.20 SP3 , Trend server is running slow, and often becomes unresponsive with high Trend Server CPU usage and its syslog.dat file contains a large amount of messages like "Exception in CiAutoFileAccess::CiAutoFileAccess", error code: 0xc0040bf3"

This situation regarding the Trend data file rollover has been identified and the fix will be included in the next Service Pack 4 for Vijeo Citect 7.20 which can be downloaded from the http://www.citect.schneider-electric.com/
Was this helpful?
What can we do to improve the information ?