Technical FAQs

Ask a Question

What is the recommendation of ground conductor for Altivar 71 drive.

The drive must be connected to the protective ground. To comply with current regulations concerning high leakage currents (above 3.5 mA),use at least a 10 mm² (AWG 6) protective conductor or 2 protective conductors with the same cross-section as the power section AC supply conductors. 
Was this helpful?
What can we do to improve the information ?