Technical FAQs

Ask a Question

Does Tesys T record operating time of Motor

The Motor operating time information is available on the Tesys T.

The information if required to be read locally , can be from the LTMCU display .

Further if required to be read on the network is available through Mapping Register 119-120 ( in secs).

Was this helpful?
What can we do to improve the information ?