Technical FAQs

Ask a Question

Will Altistart 01 work when motor is in regeneration mode.

 ATS01 will work when motor is in regeneration mode.
 If the motor become generator the motor will feed the energy to the network.
 When ATS01 is bypassed then the regenerative energy will transferred to the network in steady state condition (like DOL – direct on line starter)
 But for deceleration mode, it is not possible to feed the energy into the network. The starter controls the voltage.
Was this helpful?
What can we do to improve the information ?