Technical FAQs

Ask a Question

What is SCF4 fault on Altivar 12 drive.

SCF4 is an internal IGBT Short Circuit Fault; there is a hardware problem with the drive. Kindly replace the drive.
Was this helpful?
What can we do to improve the information ?