Technical FAQs

Ask a Question

How to Configure the IP address of Advantys OTB "OTB1E0DM9LP" from MAC Address.

Follow the below steps to set a IP address in Advantys OTB "OTB1E0DM9LP'

1) Set OTB rotary switch to Clear IP
2) Power up the unit.
3) Set Rotary switch to Stored IP
4) Power up the unit.
5) Enter the last two octets of the MAC address in the Advantys Connection settings.
Default IP address is 85.16 and last two the MAC address converted to decimal
6) Enter the permanent IP address in the Module Editor option section.
7) Connect to the Ethernet OTB through Advantys configuration software and download.
Was this helpful?
What can we do to improve the information ?