Technical FAQs

Ask a Question

What is the humidity level of Harmony XB5 pushbuttons.

All Harmony XB5 Pushbuttons conform to TH protective treatment classification. 

Limit of TH treatment is :20°C thru 55°C associated to 95% humidity level. 
Was this helpful?
What can we do to improve the information ?