Technical FAQs

Ask a Question

Is the real time and date-stamping function available when Altivar IMC integrated controller card is installed in the Altivar 71 drive.

A time and date-stamping function combined with a clock backed up by a lithium battery makes it possible to keep a log of events that have occurred. When the
Altivar IMC integrated controller card is installed in the drive, drive faults are automatically time and date-stamped without the need for any special programming. 
Was this helpful?
What can we do to improve the information ?