Technical FAQs

Ask a Question

Which type of SD Card can be used with Modicon M241 PLC series.

As per the SD Card Slot specification you can use any SD card in M241 which have SD(SDSC) or SDHC (High Capacity) upto 32 GB maximum memory and FAT32 file system formatted.
Was this helpful?
What can we do to improve the information ?