Technical FAQs

Ask a Question

What is the breaking capacity of STI isolatable fuse-carriers.

The breaking capacity of STI isolatable fuse-carriers according to IEC 60269-2 at voltage less than equal to 400 V is 50kA.
Was this helpful?
What can we do to improve the information ?