Technical FAQs

Ask a Question

Is SoMachine supported on Windows 8.1 operating system.

Yes, SoMachine V4.1 Service Pack1 is supported on following operating system:

1. Windows 7 32bit/ 64 bit
2. Windows 8.1 32bit/ 64 bit
Was this helpful?
What can we do to improve the information ?