Technical FAQs

Ask a Question

Is it possible to use 3P +N surge arrestor in 3P without Neutral in TN-C earthing System.

In TN-C system, 3P+N can be used as 3P device without using "N" connector; and connect the PE-N line to the PE connector.
The "N" cardrige will not be used.
Was this helpful?
What can we do to improve the information ?