Technical FAQs

Ask a Question

What is the difference between Intentional Delay and Max. Break time in Compact NSX VIGI module.

- The maximum breaking time (ms) is the time we can guaranty that the breaker is open
- Intentional delay is used to adjust the opening phase regarding the discrimination between breakers or specific application.
Was this helpful?
What can we do to improve the information ?