Technical FAQs

Ask a Question

What is the THDv for ATV212 drives.

THDv ((Harmonics Voltage) is not directly produced by the drive. The THDv is the result of line characteristics; it means electrical system network and THDi. 

THDv is depends on the electrical system network (impedance) and some components are:- 
Main Line Supply 
Transformer Rating 
What type of Load is connected on that supply? 

So,THDv does not totally depend on Variable Speed Drive.
Was this helpful?
What can we do to improve the information ?