Technical FAQs

Ask a Question

Is the conformal coating included as standard in Altivar 312.

ATV312 comes as a standard with conformal coated (IEC 60721-3-3 Classes 3C2 and 3S2).
Was this helpful?
What can we do to improve the information ?