Technical FAQs

Ask a Question

Is it possible to use JOG function with Brake logic control function on ATV71 drive.


JOG function is incompatible with Brake logic control function. 

Solution is to use Preset speed. Refer to attached file.
Was this helpful?
What can we do to improve the information ?