Technical FAQs

Ask a Question

What are the reasons of showing nrdy on Altistart 22 Soft Starter.

nrdy is not a fault. It is the status.
 
Following are the reasons:
 
(1) A stop command is present, with line and control power on:
LI1 = 0 and LI2 = 1 in 2-wire control
LI1 = 1 and LI2 = 1 at power up in 3-wire control
 
(2) Main power is switched off
Was this helpful?
What can we do to improve the information ?