Technical FAQs

Ask a Question

How to configure audible sound for Digital Alarms in Vijeo Citect SCADA.

To implement audible digital alarms first you have to define alarm category and alarm priority and assign that category to the Digital Alarms. 

Then define parameter from System >> Parameters >> 
Section Name :ALARM 
Name: Sound1 (1 for priority 1 alarm) 
Value : C:\WINDOWS\Media\ding.wav (Address of the sound file ) 

Then add in the INI file as [Alarm] Soundn as 
Sound1= C:\WINDOWS\Media\ding.wav 
Similary for other categories defined as sound2 , 3, 4....etc 
 
Was this helpful?
What can we do to improve the information ?