Technical FAQs

Ask a Question

Is it possible to take digital signature in Vijeo Citect

There is signature verification feature available in VJC version 7.20 and above version which provides the facility for users to approve an action or tag write operation using the new Cicode functions MultiSignatureForm and MultiSignatureTagWrite.Two further Cicode functions, VerifyPrivilegeForm and VerifyPrivilegeTagWrite, enable you to restrict access to a specific action or tag write for a user with a specific set of privileges.

This feautre can be easily checked in example project "Security page" as per the snapshot attached for your reference. 
Was this helpful?
What can we do to improve the information ?