Technical FAQs

Ask a Question

At what temperature the cooling fan of ABL1ER24100 will start/stop.

The cooling fan of power supply ABL1REM24100 will start if the temperature is higher than 40 deg C or if the current consumption is greater than 90 % of maximum load. 
Was this helpful?
What can we do to improve the information ?