Technical FAQs

Ask a Question

Is Twido Suite compatible with Windows 8 and from where can I download this software version.

This Twido programming software Twido Suite version 2.33 is compatible with Windows 8 32/64 bit .

Below is the download link & release note for the Twido Suite software version 2.33 which will also includes the driver for the USB device for Windows 8 :
Was this helpful?
What can we do to improve the information ?