Technical FAQs

Ask a Question

Can i use BMENOC 03*1 module for performing IO Scanning using Modbus TCP.

The BME NOC 03•1 Ethernet communications modules provide support for I/O scanning using EtherNet/IP and Modbus TCP. The maximum number of devices that can be shared between EtherNet/IP adapters, Modbus TCP devices, and local slaves is 128. Enclosed table present the I/O communications features of the BME NOC 03•1 module.


 
Was this helpful?
What can we do to improve the information ?