Technical FAQs

Ask a Question

How to communicate m340 plc as a profibus dp slave

You can use the Profibus Remote Master module as a profibus master on M340 range. This module can not act as a profibus slave. In the Modicon Quantum series there is an option to use our partner module from Prosoft as DP slave. Refer to the below link for complete detail on this module. 

http://www.prosoft-technology.com/Products/Schneider-Electric-In-chassis/PROFIBUS-DP-Slave-Network-Interface-Module-for-Quantum
Was this helpful?
What can we do to improve the information ?