Technical FAQs

Ask a Question

Can the line chokes and motor chokes used with the ATV38 be re-used with the ATV61.

Yes, the line chokes & motor chokes used with the ATV38 can be re-used with the ATV 61 and do not, therefore, need to be replaced. Refer to attached Migration Manual.
Was this helpful?
What can we do to improve the information ?