Technical FAQs

Ask a Question

Can i upgrade Concept processor140CPU53414B PV version 03 to Unity platform

Yes this can be done. There is no restriction on the PV number for the 140Cpu53414B. That only applies to the 534/14A and 434/12A (the restriction there has to be PV04 or later).
Was this helpful?
What can we do to improve the information ?