Technical FAQs

Ask a Question

How to set Min and Max range of bypass settings in SRC6KUXI and SRC10KUXI models?

To set Min and Max range of bypass settings in SRC6KUXI and SRC10KUXI model, follow the below instructions:

• Input supply should be on to the UPS.
• Turn on the UPS [display should be on].
• Click on ‘Enter’ button for Main Menu.
• Select the ‘Configuration’ option from Main Menu and enter on it.
• Inside the ‘Configuration’ option, find ‘bypass settings’ and enter on it.
• Enter on ‘Min bypass range’, use up/down arrow keys to set min range of voltage and click on enter to set the voltage.
• Enter on ‘Max bypass range’, use up/down arrow keys to set max range of voltage and click on enter to set the voltage.
Was this helpful?
What can we do to improve the information ?