Technical FAQs

Ask a Question

Does ATV303 drive have thermal detection.

Regarding Drive thermal detection, it is provided by a built-in PTC probe in the power module.
There is a parameter on ATV303 i.e. 809 (Drive thermal state). It displays the drive thermal state in %. Above 118%, drive displays =>Drive overheat.
Was this helpful?
What can we do to improve the information ?