Technical FAQs

Ask a Question

The UPS is not turned on (UPS:SRC6KUXI, when connected to battery, is not supplying power to the connected equipment) in battery mode.

Follow the steps,If the UPS has shutdown (the display is not on), follow
the “Cold start the UPS” 


Cold start the UPS
Step 1:Use cold start feature to supply power to connected equipment from the UPS batteries.
Step 2:Press the POWER ON/OFF button. The display panel will illuminate. Wait till the UPS
initialization is complete.
Step 3:Press and hold the POWER ON/OFF button again, until a short beep is heard, to supply
battery power to the connected equipment.
Was this helpful?
What can we do to improve the information ?