Technical FAQs

Ask a Question

What is the meaning of ASC scaling for the setting of Analogue output of ATS48 Soft Starter.

Refer to attached document; there is a formula for AO assignment.
 
For motor current, please see below: ---
 
Is = 20ma * [X(%) /ASC].
 
Where “X” represents the percentage reading compared to the nominal value selected (motor nominal current, nominal torque ...).
 
Example:
 
AO (Analog Output) => OCr : Motor current
 
O4 (Configuration of the type of signal supplied by output AO) => -020:0-20mA signal
 
ASC range is from 50 to 500% and factory setting is 200.
 
And for Example: if you program In = 120A as per Motor detail then X will be equal to 100% if 120A read by ATS48 [means=>120 A monitored by Motor Current (LCr) parameter from displayed menu (SUP)].
 
So, if ASC = 200%.
 
Then AO will be :=> 20ma * [X(%) /ASC].
 
                         => 20mA *[100/200] = 10 mA
Was this helpful?
What can we do to improve the information ?