Technical FAQs

Ask a Question

Is it possible to copy the current reference and command by means of switching on ATV61 drive.

Yes, it is possible.
There is a parameter “COP”. It can be used to copy the current reference and/or the command by means of switching.
Refer to attached file for more detail.
Was this helpful?
What can we do to improve the information ?