Technical FAQs

Ask a Question

What is INFE fault on ATV71 drive.

INFE (Internal CPU) fault appears when the microprocessor can not check his program and data.

Probable causes:
Bad initialization between motor control board and application board and asic of the power board.
 
Remedy:
Replace the control block.
Was this helpful?
What can we do to improve the information ?