Technical FAQs

Ask a Question

What is the voltage tolerance level for NSX ME VIGI.

In NSX ME VIGI the tolerances applicable to the voltage are +10% and -15%. That means the vigi works perfectly between 170V and 484V but be careful to do not pass these values.
Was this helpful?
What can we do to improve the information ?