Technical FAQs

Ask a Question

Which drives from altivar range supports RSTP protocol management

Altivar 61 and Altivar 71 range of drives with Ethernet network communication card - VW3A3320 when inserted supports RSTP management.
VW3A3320 ethernet communication card is compatible with ATV61 firmware version V5.8 and above, ATV71 firmware version V5.7 and above only.

Note:
The card - VW3A3320 can operate in half duplex or full duplex mode, whether connected to a hub or a switch and regardless of the transmission speed
(10 Mbps or 100 Mbps). RSTP function is not compatible with half duplex configuration.
 
Was this helpful?
What can we do to improve the information ?