Technical FAQs

Ask a Question

What is the maximum numbers of drives allowed on RSTP loop for Altivar 61 / Altivar 71 drives

Maximum number of drives allowed on a RSTP loop is 32 with ATV61 / ATV71.
With 32 drives it is ensured that standard IEEE802.1 is respected and a recover time less than 50ms is possible.
Was this helpful?
What can we do to improve the information ?