Technical FAQs

Ask a Question

Can I upgrade the firmware for TSX ISP Y101 module to v2.4, what are the evolutions in this version

The TSX ISP Y101 cannot be upgraded by anybody , the firmware is installed one time while manufactured. 

This new version v2.4 is not done to correct any issues. It is due to the use of a new analog digital converter component as the old one is no more manufactured. Schneider Automation has realized a new design to keep all the features of the new module identical to the old ones. But the new converter introduce a new way to supply the load cells. Before the power supply was 10V DC until SV2.3. Now the power supply is pulsed , there are pulses of +5V and pulses of -5V while the converter do the measures. First thing for customer is that now he cannot check the load cell voltage with his millimeter.

WARNING :All capacitors which could be in parallel of the load cells power supply have to be removed.
1. It will affect the measures as they introduce a delay on the front of the pulses.
2. The polarized capacitors will heat as now the load cell power supply is alternative.
Was this helpful?
What can we do to improve the information ?