Technical FAQs

Ask a Question

Cable diagram for the Telefast ABE7CPA410 module?

 The TELEFAST ABE7CPA410 sub-base is used to rapidly connect sensors to the Modicon M340 PLC. It is used to: Remotely locate input terminals in voltage mode, power 4 to 20 mA conditioning units one channel at a time with 24 V, protect and limit channels to 25 mA while maintaining their isolation, protect the current impedance matching resistors integrated in the TELEFAST against overvoltages.   

Was this helpful?
What can we do to improve the information ?