Technical FAQs

Ask a Question

Does time and Date of PM5350 meters backed to default after the control power of the meters were lost.

Kindly note that the PM5350's RTC is backed-up by a capacitor (not a battery). So if the clock is set and auxiliary power supply to the meter remains cut-off for more than 30 seconds, next time auxiliary power is restored the RTC will reset to 00:00:00 hrs (date will reset to some value), and start running henceforth. Therefore, in event of Aux. power supply interruption, user must check and set RTC as required.
Was this helpful?
What can we do to improve the information ?