Technical FAQs

Ask a Question

What is the installation consideratoion on power control connections to PowerLogic power meter's.

> Energy meter must be protected by a circuit breaker

> Energy meter must powered up by wiring it as per the diagram

> Necessary precautions to be taken for safe and controlled Power source to avoid damage to the device &/or User
Was this helpful?
What can we do to improve the information ?