Technical FAQs

Ask a Question

What are the digital output setup values available for control mode in PM5350 and provide there description.

Below are the digital output setup values available for control mode in PM5350 with there description;
• External: the digital output is controlled remotely either through software or by a PLC using commands sent through communications.
• Demand Sync: the digital output is associated with one of the demand systems. The meter sends a pulse to the digital output port at the end of every demand interval.
• Alarm: the digital input is associated with the alarm system. The meter sends a pulse to the digital output port when the alarm is triggered.
Was this helpful?
What can we do to improve the information ?