Technical FAQs

Ask a Question

What are the digital input setup values available for control mode in PowerLogic PM5500 series meter and provide there description.

Control mode field displays how the digital input functions for PowerLogic PM5500 and these are;
• Normal: the digital input is not associated with another meter function. The meter counts and records the number of incoming pulses normally.
• Demand Sync: the digital input is associated with one of the input sync demand functions. The meter uses the incoming pulse to synchronize its demand period with the external source.
• Input Metering: the digital input is associated with one of the input metering channels. The meter counts and records the number of incoming pulses and related consumption data associated with the pulses.
Was this helpful?
What can we do to improve the information ?