Technical FAQs

Ask a Question

What are modbus communication parameters available to set in PowerLogic PM5350 series meter

Digital meter Communication Settings
Protocol MODBUS RTU / Modbus ASCII / Jbus
Baud rate User set Range:9600, 19200, 38400
Parity EVEN, ODD, NONE
Device Address 1 to 247 / Upto 255 for Jbus
Was this helpful?
What can we do to improve the information ?